Other Parts Discussed in Thread: TRF7960
I'm new in RFID and I need some advice in design of RFID PCB Antenna and the RFID Tag.
I plan to use reference design based on TRF7963A and it will read ISO14443A tags in short distance (up to 1cm).
Each antenna will have its matching circuit and then will be connected to the TRF7693A reader through RF Switch in order to avoid cross talking between them.
The board should have a shape of 7 hexagons connected together(6 by the circle and 1 in center), each hexagon should have a PCB round antennas.On top layer, around or inside of antenna LEDs will be populated (6 LEDs by the circle and 1 in the center). All electronics components at the same board.
Please help me to understand my steps to achieve that:
1. Estimate PCB antenna parameters: inductance, diameter, number of loops, trice width, trace to trace distance in some simulation program.
2. Create the PCB with an estimated dimension of an antenna.
3. Measure the actual impedance with Network Analyzer and calculate value for capacitors and resistors for the matching circuit for each antenna by using Smith Chart Simulation Program.
I will appreciate any help.
Thanks.
Dmitry.