Other Parts Discussed in Thread: CC2592
The two traces on the output side of the CC2592 are different widths and have different characteristic impedances.
Both the SMA-connected device and the IFA are 50Ω loads.
1. The trace(s) from C3101 to the IFA are 0.5mm wide with 0.4mm gap over 0.175mm FR4 and simulate at 37 ohms.
2. The alternate trace from C3111 to the SMA connector is half that, at 0.25mm wide with 0.15mm gap and simulates at 54 ohms.
Why are there two different RF trace widths to 50Ω loads?
Thanks
Steve R.