This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TMS3705: I need a starting sample code

Part Number: TMS3705

Tool/software: Starterware

Hi all,

I did a breakout using the TMS3705 to read LF RFID Passive chips. The problem is that I need to test whether it works or not. To do that I just need in this step to see a data stream through SCIO pin from a oscilloscope.

1. As I understand I needs to wake up the TMS3705 and Initialize and start transmission. If I do this I will get a response from RFID passive transponder? 

2. To get a reading from the SCIO I'm need a simple C code. Please give me a SIMPLE C code just to get the reading out from SCIO Pin?

Thank you.

Dulip