Hi, everyone,
This refers to CC253x System-on-Chip Solution for 2.4 GHz IEEE 802.15.4 and ZigBee® Applications User's Guide, Pg81-84,
when P1SEL bit set to 0, the pin is a general IO pin
When P1DIR bit set to 0, it' a input, otherwise it's a output
My question is, when P1INP bit set to 1 and P1DIR bit set to input, is it disable the pull-up/ pull-down function?
When the P1DIR bit set to output, and P1INP bit set to 1, is it refer to a tri-state output pin? if yes, how to set to the High-Z mode?
Thank you very much.