Hello, I have a question related of the use of the CC1111 instead of CC1110.
I have read the documents and datahseets of CC1110/CC111. I have read that CC1110 and CC1111 can work in low-power applications operating in the 315/433/868/915MHz. But in practice it seems that this is true only in CC1110 and this is false in CC1111. It seems that CC1111 can work only in low-power applicaitons operating in 868MHz.
I need create a low-power wireless applications operating in the 433Mhz and I would like to use the CC1111 SoC because this has a full-speed USB controller. It is possible?
Thanks