Other Parts Discussed in Thread: CC2650, HDC1010
Tool/software: Code Composer Studio
Hello everyone,
I am trying program the temperature sensor Si7021 with the sensor controller on the CC2650 LAUNCHPAD. I am having a hard time understanding how to use I2C on the sensor controller studio. I have programmed the temperature sensor on Code Composer Studio successfully but I want it to run from the sensor controller so I can optimize the power consumption. Can anyone help me better understand the use of I2C on sensor controller. I have looked at the Ambient light sensor example that they have but I do not understand it.
/*
* ======== empty.c ========
*/
/* XDCtools Header files */
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/power/PowerCC26XX.h>
/* BIOS Header files */
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
/* TI-RTOS Header files */
#include <ti/drivers/I2C.h>
#include "I2C.h"
#include <ti/drivers/PIN.h>
#include <ti/drivers/i2c/I2CCC26XX.h>
#include <driverlib/prcm.h>
/* Board Header files */
#include "Board.h"
#define TASKSTACKSIZE 1024
Task_Struct task0Struct;
Char task0Stack[TASKSTACKSIZE];
Void Si7021(UArg arg0, UArg arg1)
{
I2C_init();
// Local Variables
uint8_t txBuff[1];
uint8_t rxBuff[2];
I2C_Handle handle;
I2C_Params params;
I2C_Transaction transaction;
char i = 0;
bool ret;
I2CCC26XX_I2CPinCfg pinCfg;
// Opening the driver
I2C_Params_init(¶ms);
params.bitRate = I2C_400kHz;
// Initialize master I2C transaction structure
transaction.writeCount = 1;
transaction.writeBuf = txBuff;
transaction.readCount = 2;
transaction.readBuf = rxBuff;
transaction.slaveAddress = 0x40;
// Open the I2C
handle = I2C_open(Board_I2C0, ¶ms);
// Check for I2C Initialization
if(handle == NULL)
{
System_printf("Error initializing\n");
}
else
{
System_printf("I2C initialized\n");
}
System_flush();
pinCfg.pinSDA = Board_I2C0_SDA0;
pinCfg.pinSCL = Board_I2C0_SCL0;
params.custom = (uintptr_t)&pinCfg;
// Extract data from sensor
while(TRUE)
{
System_printf("Case %d: \n", i + 1);
//System_flush();
txBuff[0] = 0xE5;
ret = I2C_transfer(handle, &transaction);
if(ret)
{
// Get data from the buffers
uint16_t msb = rxBuff[0];
uint16_t lsb = rxBuff[1];
//lsb &= 0xFC;
uint16_t hum = msb << 8 | lsb;
// Convert the data to readable data
float humidity = (125.0 * hum);
humidity /= 65536;
humidity -= 6;
System_printf("%1.2f percent RH\n", humidity);
System_flush();
}
txBuff[0] = 0xE0;
if(ret)
{
//Get data from the buffers
uint16_t msb = rxBuff[0];
uint16_t lsb = rxBuff[1];
//lsb &= 0xFC;
uint16_t temp = msb << 8 | lsb;
// Convert the data to readable data
float temperature = (175.72 * temp);
temperature /= 65536;
temperature -= 46.85;
// Convert to Fahrenheit
temperature *= 9;
temperature /= 5;
temperature += 14;
System_printf("%1.2f degrees F\n", temperature);
System_flush();
}
i++;
}
}
/*
* ======== main ========
*/
int main(void)
{
Task_Params taskParams;
/* Call board init functions */
Board_initGeneral();
Board_initI2C();
/* Construct heartBeat Task thread */
Task_Params_init(&taskParams);
taskParams.stackSize = TASKSTACKSIZE;
taskParams.stack = &task0Stack;
Task_construct(&task0Struct, (Task_FuncPtr)Si7021, &taskParams, NULL);
/* Start BIOS */
BIOS_start();
return (0);
}
I have inserted the code I used to program the temperature sensor using code composer studio. If anyone can please help me convert this code to something that will function on the sensor controller studio. Thank you!
Best Regards,
Francisco Ochoa