Part Number: TRF7970A
Hi.
I'm using the TRF7970A in SPI and I'm having a problem with some component.
After a power down the initialization of the TRF fails and no tag reading is possible
you have to turn off the power for more than 2 seconds and at power on initialization works.
EN is driven by the μc EN2 is connected to VSS
My init sequence:
Power on
EN = 0 ;
Delay 100ms
EN = 1;
delayEnMs(20) ; // wait tempo 20ms until system clock started
mod_control[0] = SOFT_INIT; // 0x03
SpiTrf797xDirectCommand(mod_control);
mod_control[0] = IDLE; // 0x00
SpiTrf797xDirectCommand(mod_control);
mod_control[0] = MODULATOR_CONTROL; // 0x09
mod_control[1] = 0x09; // OOK 100%, ASK/OOK as an analog output
SpiTrf797xWriteSingle(mod_control, 2);
mod_control[0] = MODULATOR_CONTROL;
SpiTrf797xReadSingle(mod_control, 1);
if (mod_control[0] != mod_control[1])
{
// defaut init
res = 0;
}
Can you help me