Part Number: CC8530
Yes, I have searched the forums and seen the posts related to this issue.
However, I am asking a question that seems unique from those. I want several (e.g. 4) audio producer channels (slaves) to provide input to several different masters. For example, multiple mic slaves providing the same input to several loudspeakers (masters). NOT 4 channels to one master and 4 to another to give 8 channels to one base station possessing two master chips, BUT RATHER 4 channels simultaneously to multiple listening base stations each with one master chip.
I want to know if I can pull this off with CC85XX technology. It should be doable in concept. I can see that I would need some time-slot assignment for multiple master Tx. I don't need that - one "Master among masters" could handle all I'd need for Tx to slaves - but I want the second-tier masters to have simultaneous access to the audio content (Rx) for rendering. I don't want to have to set up a whole other system to re-transmit from a "master speaker" to the others. I theory, reception by one master can't prevent the other masters from hearing the same signal, right? it's the timing that concerns me.
Also, I'm trying to avoid duplicate (or more) Tx chips in each slave source. First, space in a mic is at premium. Also, I'd like to have an arbitrary number of (in range) listening masters without and extra chip set inside each mic to service. Again, only one master ever needs to Tx to mic(s) - and I don't think I even need that unless it's part of the error check protocol.
Thanks for input,
-Rick