This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/DLP-7970ABP: ''RF7970A boosterpack'' P2P connection using MSP-430G2 (MSP430G2553) lunchpad

Part Number: DLP-7970ABP
Other Parts Discussed in Thread: MSP430G2553, TRF7970A, MSP430F5529

Tool/software: Code Composer Studio

Hello

I want to establish a P2P connection between two TRF7970A boosterpack which are implemented on two  MSP-430G2 (MSP430G2553) launchpads and  i have following questions about it.

1.TRF7970A: MSP430G2 Firmware provided, can only implement iso 14443a/b and iso 15693, not iso 18092 (required for P2P). is it possible to implement P2P connection with these hardware? 

2. if its possible please provide me with useful information and links.

considering that ,this P2P connection is implemented using MSP430F5529 LaunchPad and TRF7970A boosterpack , the thing is , i want to use MSP-430G2 (MSP430G2553) launchpads and i want to have only  P2P connection.

thanks