Part Number: TRF7970A
Other Parts Discussed in Thread: DLP-7970ABP
I've been assigned a project using RFID for one of our product lines. So, I started out with the MSP432P401R launchpad along with the DLP-7970ABP booster pack and the NFC/HF RFID Reader / Writer application(SLOA227A). Everything works great and I've learned a great deal. Now the scope of the project has changed and we now want to use the DESFire tags because of the high level of encryption. So, I found the DESFire EV1 AES Authentication app., SALOA213 and quickly realized that I had to port the code so that I could use it on the MSP432. Everything was going fine until I ran into the MFDESFire folder in the project and the AES_Encryption library. I need to rebuild the AES_Encryption.lib library to run on the MSP432 and there's no source code. Were can I find it?? I've looked all over and have been unable to locate it. Could some someone please point me in the correct direction?