This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: Whether CC1352 is supporting proprietary 2.4GHz mode or not?

Part Number: CC1352R
Other Parts Discussed in Thread: CC1352P

We are  looking for a single solution which can support SubGhz, IEEE802.15.4 in 2.4Ghz and proprietary 2.4GHz mode.

Unlike the CC2652, it is not clearly mentioned in the data sheet whether CC1352 is supporting proprietary 2.4GHz mode or not.

We want 2Mbps 4-GFSK in 2.4GHz with CC1352. Is it possible?