Part Number: CC2545
Dear All,
According to TI CC2545 User Guide Page 236, Section:23.5 Frequency and Channel Programming:
"
For normal transmit and receive tasks, the carrier frequency is set by using the register PRF_CHAN.FREQ.
The carrier frequency is 2379 + n MHz, where n is the value of this register, where n can be from 0 to 116.
This gives a frequency range from 2379 MHz to 2495 MHz. Note that this frequency range extends
beyond the ISM band. If PRF_CHAN.FREQ is set to 127, and for the Rx and Tx test commands, the
frequency must instead be programmed directly in hardware registers.
In this case, the synthesizer frequency is set by programming the 7 bit frequency word located in
FREQCTRL.FREQ[6:0]. The synthesizer frequency is given by 2379+ nMHz, where n is the value of
FREQCTRL.FREQ[6:0], and is programmable in 1-MHz steps. The device supports synthesizer
frequencies in the range from 2379 MHz to 2495 MHz. The usable settings for freq[6:0] is consequently 0
to 116.
In Rx, the system operates on a low intermediate frequency (IF) of 1 MHz for data rates up to 1 Mbps, and
on a zero IF for 2 Mbps. In Tx, the system supports operating on low IF or zero IF. The IF to be used for
Tx can be programmed in the register MDMTEST1.TX_TONE. The receiver may operate on a positive of
negative IF when the data rate is 1 Mbps and lower; this is controlled with MDMTEST1.RX_IF.
When the symbol rate is 1 Mbps or lower and the LLE programs the frequency, it uses a ±1 MHz IF on Tx.
For both Rx and Tx, a negative IF is used when PRF_CHAN.FREQ < 62 and a positive IF is used when
PRF_CHAN.FREQ ≥ 62
When the symbol rate is 2 Mbps and the LLE programs the frequency, it uses an IF on Tx as specified in
PRF_RADIO_CONF.TXIF. This IF may be zero, or ±1 MHz, ±2 MHz, or ±3 MHz. The recommended
setting is ±1 MHz. A negative IF is used when PRF_CHAN.FREQ < 62 and a positive IF is used when
PRF_CHAN.FREQ ≥ 62.
For all data rates, the setting of MDMCTRL1.PHASE_INVERT is taken into account by the LLE when finding
the setting for MDMTEST1.TX_TONE. The FREQCTRL register will be programmed corresponding to the
programmed IF in order to operate on the channel specified by PRF_CHAN.FREQ.
."
My questions is:
[1] How many number of channels are possible within 2400 - 2483.5 ISM band if I use 1Mbps and/or 2 Mbps Data rates.
[2] Could I change Channel Spacing for both 1 Mbps or 2 Mbps. Do CC2545 support channel spacing settings.?
I have consulted Datasheet and User guide but i am still confused some brief description will be appreciated. Thank you