This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FLASH-PROGRAMMER: CLI Programmation time most longer than GUI Programmation time

Part Number: FLASH-PROGRAMMER
Other Parts Discussed in Thread: CC2630, CC1350

Hi everybody

I have a question

I compare the time to programme a cc2630

I used Flashprogrammer 2 to erase-program and verify CRC

The time to made this action is approx 5s

after this I write 4 byte in page 31

The time to made this action is approx 5s

But when I made action with CLI

srfprog.exe -t soc(XDS-00000000,cc2630) -e all -p -v -f E:\Industrialisation\XCMW radio\trunk\Outils\Programmation avec XDS100\XCMW_v1.0.out -rs none

The time to made this action is approx 15s

and

srfprog.exe -t soc(XDS-00000000,cc2630) -r p(31) -f E:\Industrialisation\XCMW radio\trunk\Outils\Programmation avec XDS100\readback.bin

The time to made this action is approx 13s

Why?

How can I have the command used by GUI to made action?

Thanks in advance for your help