Hello
I'm having a small range problem using the TRF7960 and the tiny Murata rfid chip (LXMS33HCNG). Is it possible to power the TRF7960 PA only with 5V leaving the rest of the chip powered by 3v3 so that the MCU interface can be left at 3v3, to boost the output? And if doing so, do I need to set the 5V operation bit in the status control register to get anything out of it?
/Mikael