Part Number: CC8520
Other Parts Discussed in Thread: CC8521, CC2590, CC2591
Hello all,
Having exhausted my avenues, turning to you for advice.
I have had PCBs made from the Gerber files of the CC85XX-CC2590EM Reference Design.
Have built five of these boards, all of which I can program and they do come up with LED blinking in 'alone' mode.
However, no joy at pairing.
Have used fixed pairing based on master deviceID (I confirm the IDs are correct).
Have tried with external antenna (SMA connector) and with the onboard antenna (in both cases leaving C114 unpopulated)
The deviceID of the master (a CC8521) is 0x203BCB44
I do have access to a scope, but before going down that route wanted to check if I am missing something obvious.
The purepath configurator files I am using are attached.
The voltage on XPAEN pin is around 0.6. I cannot see any obvious electrical / soldering errors.
Any help/pointers greatly appreciated!