Other Parts Discussed in Thread: CC2520
Greetings,
I'm working on your official reference guide with the source code made for MSP2618. I've created a working port of the interface for STM32F407VGT and currently trying to get the per_test.c project to work. I've printed a PCB board according to the TI reference design (almost the same as http://www.ti.com/tool/cc2520emk ) which is connected to the STM32F4. The transmitter is one STM32F4+CC2520 breakout, and the receiver is an another STM32F4 with its own CC2520 breakout board.
The entire project is -functional- with SPI commands working, register read, write instructions also working. I can configure CC2520-GPIO lines to any of the available exceptions/signals and so on.
But when I issue SRXON strobe command, I can see that the device is in RX mode (RX_ACTIVE flag on GPIO5 for me), but when I try to send another strobe over SPI, the entire chip resets - all internal registers are back to default state. The EXCFLAGx registers inform me that RX_OVERFLOW and SPI_ERROR exceptions have appeared, but the RXFIFOCNT is 0x00 and no other indicators of successful RX have appeared.
Is there a special treatment for SRXON command which should be taken into consideration? It seems like it messes up the SPI interface for the next command, whether I attempt to read from status registers, or request a SNOP strobe or anything else.
To sum up:
When I send an SRXON strobe, chip enters RX mode.
After I send a new command over SPI ( after SRXON, instantly or after a certain delay), the chip resets completely - including the initial GPIOCTRLx configuration.
Everything else works: All expected functionalities over SPI and related to GPIO lines.
How can I overcome this issue?
Kind regards,
Dominik Perkovic