hi All,
I have project with CC2530 RF chip. I have write application which Tx / Rx files between two EV boards CC2530. I have used two PCs with Hyper termial application(UART) and Kermit protocol.
The problem is that I could not speed up the bps more than 8K(I have used SimpleTI stack protoocl). The chip is suppose to work on 250K bps.
Could someone know how could I speed up the bps?
Is someone have succedded to work on 250K bps as the chip is should be worked?
Thx,
Simbad