Other Parts Discussed in Thread: CC2590
My customer is searching TI's wireless digital audio streaming scheme.
Their demand is as follows:
(1) The communciation range is beyond 30m with no error concealment.
(2) As their sample rate can be down to 24K, they said the decoding course can be carried out by the main controller if there is no wireless SoC.
(3) The latency is lower than 1ms for the best, 10ms is also OK.
(4) Their system would have one master, two or more slave audio sets.
I see that TI has PurePath Wireless 2.4 GHz RF SoC for wireless digital audio streaming.
My quesiton is, Is there any other suggestion for the customer's demand?