Other Parts Discussed in Thread: CC1101
Hello,
I have a Projekt in my University. Its about the Current Consumption of the CC1101.
We combine the CC1101 with levelshifter and an Arduino Uno .
So i dont have the Chance to use the RFstudio from TI.
Whats so ever, i got problem with implementing ASK/OOK Modulation. I just read some Threads here, but non of the settings from it will help me.
Everthing is fine with GFSK,2-FSK,4-FSK but ASK/OOK won't work. I also read the DN022 Document, but these settings seems also not to work.
I read about wrong RX Channel BW and wrong Output Power, but non of it would work. I also changed distance between the Transievers. Pls help me !
I'm also not sure about that Patable Table i read about, maybe i got understanding Problems ( do i have to get the Table in my source coud or into the Liberary ? for example :
byte PA_TABLE[]= {0x00,0x60,0x00,0x00,0x00,0x00,0x00,0x00,};)
Output Power = 0 dbm
Channel Bw = 203 KhZ
Deviation = 20,63 kHz
Channel Spacing = 199,951 kHz
Data Rate = 38,3835 kBaud
Sync word qualifier mode = 30/32 sync word bits detected
CRC enable = true
// Carrier frequency = 433 MHz #define CC1101_DEFVAL_FREQ2_433 0x10 // Frequency Control Word, High Byte #define CC1101_DEFVAL_FREQ1_433 0xA7 // Frequency Control Word, Middle Byte #define CC1101_DEFVAL_FREQ0_433 0x62 // Frequency Control Word, Low Byte #define CC1101_DEFVAL_MDMCFG4 0x8A // Modem Configuration #define CC1101_DEFVAL_MDMCFG3 0x83 // Modem Configuration #define CC1101_DEFVAL_MDMCFG2 0xB3 // Modem Configuration #define CC1101_DEFVAL_MDMCFG1 0x22 // Modem Configuration #define CC1101_DEFVAL_MDMCFG0 0xF8 // Modem Configuration #define CC1101_DEFVAL_DEVIATN 0x35 // Modem Deviation Setting #define CC1101_DEFVAL_MCSM2 0x07 // Main Radio Control State Machine Configuration //#define CC1101_DEFVAL_MCSM1 0x30 // Main Radio Control State Machine Configuration #define CC1101_DEFVAL_MCSM1 0x20 // Main Radio Control State Machine Configuration #define CC1101_DEFVAL_MCSM0 0x18 // Main Radio Control State Machine Configuration #define CC1101_DEFVAL_FOCCFG 0x16 // Frequency Offset Compensation Configuration #define CC1101_DEFVAL_BSCFG 0x6C // Bit Synchronization Configuration #define CC1101_DEFVAL_AGCCTRL2 0x04 // AGC Control //#define CC1101_DEFVAL_AGCCTRL2 0x43 // AGC Control #define CC1101_DEFVAL_AGCCTRL1 0x00 // AGC Control //#define CC1101_DEFVAL_AGCCTRL1 0x40 // AGC Control #define CC1101_DEFVAL_AGCCTRL0 0x91 // AGC Control #define CC1101_DEFVAL_WOREVT1 0x87 // High Byte Event0 Timeout #define CC1101_DEFVAL_WOREVT0 0x6B // Low Byte Event0 Timeout #define CC1101_DEFVAL_WORCTRL 0xFB // Wake On Radio Control //#define CC1101_DEFVAL_FREND1 0x56 // Front End RX Configuration #define CC1101_DEFVAL_FREND1 0xB6 // Front End RX Configuration #define CC1101_DEFVAL_FREND0 0x10 // Front End TX Configuration #define CC1101_DEFVAL_FSCAL3 0xE9 // Frequency Synthesizer Calibration #define CC1101_DEFVAL_FSCAL2 0x2A // Frequency Synthesizer Calibration #define CC1101_DEFVAL_FSCAL1 0x00 // Frequency Synthesizer Calibration #define CC1101_DEFVAL_FSCAL0 0x1F // Frequency Synthesizer Calibration #define CC1101_DEFVAL_RCCTRL1 0x41 // RC Oscillator Configuration #define CC1101_DEFVAL_RCCTRL0 0x00 // RC Oscillator Configuration #define CC1101_DEFVAL_FSTEST 0x59 // Frequency Synthesizer Calibration Control #define CC1101_DEFVAL_PTEST 0x7F // Production Test #define CC1101_DEFVAL_AGCTEST 0x3F // AGC Test #define CC1101_DEFVAL_TEST2 0x81 // Various Test Settings #define CC1101_DEFVAL_TEST1 0x35 // Various Test Settings #define CC1101_DEFVAL_TEST0 0x09 // Various Test Settings
Thanks & Best Regards,
Andi