Other Parts Discussed in Thread: CC1310, LAUNCHXL-CC1310
Hi everyone,
I just received two SmartRF06 EVB with two CC13XXEM boards. I also received 3 Sub-1 GHz CC1310 LaunchPad boards.
I would like to program the two CC13XXEM boards + the CC1310 LaunchPad boards with a software that was provided to me
from TI. My question is, can I program these boards with the following: SmartRF Flash Programmer 2 software? My second
question is, since they sent me the entire file, which file do I have to use? Third question is, if I can use the SmartRF Flash Programmer 2
is there documentation on this?
Thanks,
Neil