Part Number: RF37S114
RF gurus - This is a question for one of my customers.
I have read the following e2e post (
) as well as the “Reader Antenna Optimization for Reading the RF37S114” document (
)
and that document seems to be saying the tag is going to max out at about 1.5 cm read range. Is that the best I can expect from this part? "We are hoping for more like 2 inches."
The protocol of the part is ISO 15693, and this protocol is intended for extended read ranges, like up to 1 meter. They are called “vicinity” tags rather than “proximity” tags. Using a standard reader (about 1.5”x1” area), and I am limited to 1/4 inch read distance – probably due to the small tag area, but the customer wants to know if longer range is possible with a better reader.
Thanks!