Part Number: CC8520
Hello,
Our certification lab is looking into compliance with FCC 15.247, a(1)(iii), it says:
Frequency hopping systems in the 2400-2483.5 MHz band shall use at least 15 channels. The average time of occupancy on any channel shall not be greater than 0.4 seconds within a period of 0.4 seconds multiplied by the number of hopping channels employed. Frequency hopping systems may avoid or suppress transmissions on a particular hopping frequency provided that a minimum of 15 channels are used.
Here is what we know about our system:
- The unit has 18 hopping channels, that means the average time of occupancy shall not greater than 0.4s within 7.2s period.
- We also know that the transmissions sent by the Master and Slave both are variable in length between a minimum and maximum duration. We also know that the maximum duration transmission happens immediately after the Slave joins the network. We have measured the maximum duration to be 1.14ms.
- We know that in a given 100ms time period, the unit will transmit on a given frequency a maximum of 8 times. (There are 40 timeslots in a 100ms period, 1/5 of these timeslots are devoted to each Active Channel)
- Combining #2 & #3, we can calculate a worst case duty cycle of 9.12% (8*1.14ms)/100ms
- If we hold the worst case duty cycle over the entire 7.2s period from #1, the time of occupancy over that period would be 7.2*9.12%=0.66s which is over the 0.4second limit
I am confident that the units do not actually transmit at the maximum 1.14ms duration over the entire 7.2sec period, but I'm not sure how to actually demonstrate compliance. Has TI looked at this before?
Thanks,
Arthur