Part Number: CC8531
Dear TI experts:
We connected an LED and a 1K resistor between VCC 3.3V and GIO3 of CC8531, then config GIO3 to working status indication in PPW Configurator, then use scope to check the output of GIO3 when LED blinking (in idle state). We found the low level output of GIO3 is almost 1V, it is too high to be recognized as a logic '0', then we changed the resistor to 10K to reduce the load current pulled by GIO3 when low level, but still saw a nearly 1V low level.
We did not find the output capability definition in CC8531's datasheet and user manual, so can anyone help to let us know how much current the GIO3 (when use as LED state indication) can sink?
Thanks.
Walter