Hi
Our customer uses TRF7963A, a tag is NTAG213 which complies to ISO14443A
In operation, our customer faced mismatch of UID.
NTAG213 has 7Byte UID, for example, 04 0C AC 12 ED 4C 81.
I describe example of UID mismatch.
UID : 04 0C AC 12 ED 4C 81
Reading UID : 88 04 0C 12 FF FF FF
The value of "88" in reading UID seeems to have meaning because
it is CT (Cascade TAG) which is defined in NTAG213 datasheet.
Regarding to appearing "FF FF FF" and "AC" is disappeared, I have no idea.
Questions.
1.
When TRF7963A read tag, is it normal operation that CT is included in UID?
2.
Is there possibility that the anticollision process would affect to read tag?
In customer system, a single tag should be read. So we don't need to acitvate anticollision.
Could you please give us your feedback?
BestRegards