Other Parts Discussed in Thread: CC2592
Hi folks, in ZNP the file mac_radio_defs.c has some tables in which some values are with a TBD (to be defined) comment, in a particulary way the values that under HAL_PA_LNA_CC2592 ||MAC_RUNTIME_CC2592 MACRO. This is set for many versions of ZNP, so I have filled out with the following values, Are they correct?
- macRadioDefsRssiAdj: -10, -5;
- macRadioDefsSensitivityAdj: -3;
- macRadioDefsSaturationAdj: -12;