Part Number: CC3200MOD
Other Parts Discussed in Thread: CC3220S, CC3200
Hi There,
I am developing IoT application where I am aiming to build Mesh network using ZigBee (may be). All the end devices should be able to connect to Mesh node.
Ultimate aim is to provide internet access to the end devices and for that I believe I have to have a WiFi Gateway which is connected to internet using GSM/GPRS and provides end devices internet access.
While searching the net I came across CC3200MOD.
Appreciate further information on this to see if it serves purpose I am looking for.
Also, few queries regarding the chip,
1. What I understand about this chip is, it acts as access point. Connected MCU can configure the policies and security parameters for establishing connection. Based on configuration it accepts connection to other devices and in-turn provide internet access. I believe, MCU just need to configure the parameters and it does not play any role in data path. ie. once connection is established, data access for the end device is seamless and MCU does not play any role. Is my understanding right?
2. Do you provide protocol stack and Drivers as part of SDK?
2. Is this chip a right suite to work for Mesh network kind of application? Do you have any suggestion?
3. Do you have any further suggestion in selecting ZigBee node ?
Looking forward for your quick response!
TIA.
Thanks
/Hp