Other Parts Discussed in Thread: WL18XXCOM82SDMMC, WL1835MOD, WL1835
Hi,
I am using the WL1835MODCOMB with the WL18XXCOM82SDMMC adapter card. With HCITool I can send the correct firmware and execute the HCI commands. I can also check the execution with Logger 5.0.
Now I would like to use LQM to see the level of the broadcast signal. What are the commands to execute to have a display on LQM?
I can not connect to the COM4 port because it is already used with HCITool. What is the COM port to use?
I tried :
Send_HCI_VS_Read_RSSI 0xFDFC, 0x01
Sender TX / RX packet:
Send_HCI_VS_DRPb_Tester_Packet_TX_RX 0xFDCC, 0, 3, 2402, 0xFFFF, 2, 0, 27, 7, 1, 0x01FF
Wait_HCI_Command_Complete_VS_DRPb_Tester_Packet_TX_RX_Event 5000, any, HCI_VS_DRPb_Tester_Packet_TX_RX, 0x00
But still nothing about LQM.
Thank you in advance for your help.