Hi
My Receiver does not received data from TX
This is my setup
Receiver
Network role : Master
Application role :Stereo output base station
Operation : Host control
Audio Interface : DSP, 24bit I2S with MCLK
Audio Streaming : (slave to master) Input left / right , Audio IO : AD0
Streaming format : PCME24
Tx
Network role : Slave
Application role : Stereo input satellite
Operation : Host control
Audio Interface : DSP, 24bit I2S with MCLK
Audio Streaming : (slave to master) Input left / right , Audio IO : AD0 , ACH_SET_USAGE 0, 1
After link, when I check the AD0 port in Tx, I can see I2S data format, but In receiver, there is no Data, just low value.
Is there some problem? Actually, I'm using AD0 for TX and Receiver.
And I want to use 2 mic system , So I choose Tx slave.