This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Reading serial inputs

Part Number: CC2650

Hello everyone,

I need to read the serial input(DIO3) while udp-client process running on cc2650. If anyone knows how to edit the code please help me.udp-client.c is as follows,I only needs to when a packet send just read the available serial input / previous input ad send them with the packet. If anyone knows how to code this inside the code  please edit this code and paste.much helpful. 

#include "contiki.h"
#include "lib/random.h"
#include "sys/ctimer.h"
#include "net/ip/uip.h"
#include "net/ipv6/uip-ds6.h"
#include "net/ip/uip-udp-packet.h"
#include "sys/ctimer.h"
#ifdef WITH_COMPOWER
#include "powertrace.h"
#endif
#include <stdio.h>
#include <string.h>

#define UDP_CLIENT_PORT 8765
#define UDP_SERVER_PORT 5678

#define UDP_EXAMPLE_ID 190

#define DEBUG DEBUG_PRINT
#include "net/ip/uip-debug.h"

#ifndef PERIOD
#define PERIOD 60
#endif

#define START_INTERVAL (15 * CLOCK_SECOND)
#define SEND_INTERVAL (PERIOD * CLOCK_SECOND)
#define SEND_TIME (random_rand() % (SEND_INTERVAL))
#define MAX_PAYLOAD_LEN 30

static struct uip_udp_conn *client_conn;
static uip_ipaddr_t server_ipaddr;

/*---------------------------------------------------------------------------*/
PROCESS(udp_client_process, "UDP client process");
AUTOSTART_PROCESSES(&udp_client_process);
/*---------------------------------------------------------------------------*/
static void
tcpip_handler(void)
{
char *str;

if(uip_newdata()) {
str = uip_appdata;
str[uip_datalen()] = '\0';
printf("DATA recv '%s'\n", str);
}
}
/*---------------------------------------------------------------------------*/
static void
send_packet(void *ptr)
{
static int seq_id;
char buf[MAX_PAYLOAD_LEN];

seq_id++;
PRINTF("DATA send to %d 'Hello %d'\n",
server_ipaddr.u8[sizeof(server_ipaddr.u8) - 1], seq_id);
sprintf(buf, "Hello %d from the client", seq_id);
uip_udp_packet_sendto(client_conn, buf, strlen(buf),
&server_ipaddr, UIP_HTONS(UDP_SERVER_PORT));
}
/*---------------------------------------------------------------------------*/
static void
print_local_addresses(void)
{
int i;
uint8_t state;

PRINTF("Client IPv6 addresses: ");
for(i = 0; i < UIP_DS6_ADDR_NB; i++) {
state = uip_ds6_if.addr_list[i].state;
if(uip_ds6_if.addr_list[i].isused &&
(state == ADDR_TENTATIVE || state == ADDR_PREFERRED)) {
PRINT6ADDR(&uip_ds6_if.addr_list[i].ipaddr);
PRINTF("\n");
/* hack to make address "final" */
if (state == ADDR_TENTATIVE) {
uip_ds6_if.addr_list[i].state = ADDR_PREFERRED;
}
}
}
}
/*---------------------------------------------------------------------------*/
static void
set_global_address(void)
{
uip_ipaddr_t ipaddr;

uip_ip6addr(&ipaddr, 0xaaaa, 0, 0, 0, 0, 0, 0, 0);
uip_ds6_set_addr_iid(&ipaddr, &uip_lladdr);
uip_ds6_addr_add(&ipaddr, 0, ADDR_AUTOCONF);

/* The choice of server address determines its 6LoPAN header compression.
* (Our address will be compressed Mode 3 since it is derived from our link-local address)
* Obviously the choice made here must also be selected in udp-server.c.
*
* For correct Wireshark decoding using a sniffer, add the /64 prefix to the 6LowPAN protocol preferences,
* e.g. set Context 0 to aaaa::. At present Wireshark copies Context/128 and then overwrites it.
* (Setting Context 0 to aaaa::1111:2222:3333:4444 will report a 16 bit compressed address of aaaa::1111:22ff:fe33:xxxx)
*
* Note the IPCMV6 checksum verification depends on the correct uncompressed addresses.
*/

#if 0
/* Mode 1 - 64 bits inline */
uip_ip6addr(&server_ipaddr, 0xaaaa, 0, 0, 0, 0, 0, 0, 1);
#elif 1
/* Mode 2 - 16 bits inline */
uip_ip6addr(&server_ipaddr, 0xaaaa, 0, 0, 0, 0, 0x00ff, 0xfe00, 1);
#else
/* Mode 3 - derived from server link-local (MAC) address */
uip_ip6addr(&server_ipaddr, 0xaaaa, 0, 0, 0, 0x0250, 0xc2ff, 0xfea8, 0xcd1a); //redbee-econotag
#endif
}
/*---------------------------------------------------------------------------*/
PROCESS_THREAD(udp_client_process, ev, data)
{
static struct etimer periodic;
static struct ctimer backoff_timer;
#if WITH_COMPOWER
static int print = 0;
#endif

PROCESS_BEGIN();

PROCESS_PAUSE();

set_global_address();

PRINTF("UDP client process started\n");

print_local_addresses();

/* new connection with remote host */
client_conn = udp_new(NULL, UIP_HTONS(UDP_SERVER_PORT), NULL);
if(client_conn == NULL) {
PRINTF("No UDP connection available, exiting the process!\n");
PROCESS_EXIT();
}
udp_bind(client_conn, UIP_HTONS(UDP_CLIENT_PORT));

PRINTF("Created a connection with the server ");
PRINT6ADDR(&client_conn->ripaddr);
PRINTF(" local/remote port %u/%u\n",
UIP_HTONS(client_conn->lport), UIP_HTONS(client_conn->rport));

#if WITH_COMPOWER
powertrace_sniff(POWERTRACE_ON);
#endif

etimer_set(&periodic, SEND_INTERVAL);
while(1) {
PROCESS_YIELD();
if(ev == tcpip_event) {
tcpip_handler();
}

if(etimer_expired(&periodic)) {
etimer_reset(&periodic);
ctimer_set(&backoff_timer, SEND_TIME, send_packet, NULL);

#if WITH_COMPOWER
if (print == 0) {
powertrace_print("#P");
}
if (++print == 3) {
print = 0;
}
#endif

}
}

PROCESS_END();
}
/*---------------------------------------------------------------------------*/