Tool/software: Code Composer Studio
Hello everyone.
TRF7970A chip continues make make me crazy. How hard to learn it.
I did not achive to pass authentication 14443A MIFARE CLASSIC TAG. And I tracked problem with logic analysor.
Problem is that, there is no any SDM Bit Clock pulse from TRF to MCU. Activatig TAG is OK because I saw 4 byte UID on my LCD and UID is corrected
with M302 RFID reader/writer.
MCU : FR6989
DCO Freq : 8 MHz
MCLK Freq : 8 MHz
SMCLK :8 MHz
SPI Freq : SMCLK / 4 = 2 MHz
Code derived from : SLOA214 DOC
Best regards.....