This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8530: CC8530: More general device ID settings in PP Wireless Configurator

Part Number: CC8530

Hello Forum Fellows:

We have developed a product using the CC8530, with one Protocol Master (PM) and four Protocol Slaves (PS).

I am using the PM in host controlled mode, and down load it's program from a uP using the SPI port. This works as advertised.

(The PM board does not have a JTAG connector to program the CC8530 device.)

I program each of the PSs using the PurePath Wireless Configurator (PPWC) and that also works OK.

(The PS boards do not have a paring button.)

I would like more flexibility attaching the slaves to the master.

Currently, I must glean the "Default Network ID" in the PM using the uP and the DI_GET_DEVICE_INFO command.

Then I must manually put that into the PPWC and program the PSs.

While this works, it is too restrictive.

I would like to allow any receiver in range to connect to any master.

Observations:

In the PPWC help I note the paragraph...

For protocol slaves only: Specify the default network ID, i.e. the 32-bit unique address of a master device. The values 0x00000000 and 0xFFFFFFFF have special meanings and must not be used. The value 0xFFFFFFFE disables the default network ID.

I find I cannot enter 0xFFFFFFFF in the PS "Default Network ID" field.

Notes:

There is no pairing button on any of the 5 devices, so under the option "Paring Trigger" I think I must select "None (fixed network ID)"

However, if I select "Button", I find under "Paring Mechanism" one of the options is Proximity. Will this work for my needs? I note I must still enter a Default Network ID.

Thanks for any insight you can offer.

Mark.