Part Number: CC2533
Hi Team,
A customer has been testing battery monitor with CC2533 for a while, and he met some problem.
He uses our example code [as follows]. The value to monitor is 2.146v, it can be monitored if use a regulated source to jump the voltage to 2.146v. But if make a low temperature experiment[-40℃], some boards will print a not accurate voltage. Is the battery monitor influenced by temperature?
The code is below:
uint8 HalBatMonRead(uint8 vddMask)
{
uint8 rtrn = TRUE;
#if (HAL_BATMON == TRUE)
MONMUX = 0; // Setup BATTMON mux to measure AVDD5.
BATMON = vddMask;
halMcuWaitUs(2); // Wait at least 2 us before reading BATTMON_OUT.
rtrn = (BATMON & BATTMON_OUT) ? TRUE : FALSE;
BATMON = BATTMON_PD; // Turn off for power saving.
#endif
return rtrn;
}
//user guid P142
/*
------------- step 0.024
3: 1.93v
4: 1.954v
5: 1.978v
6: 2.002v
7: 2.026v
8: 2.050v
9: 2.074v
10: 2.098v
11: 2.122v
12: 2.146v
13: 2.170v
14: 2.194v
15: 2.218v
16: 2.242v
17: 2.266v
18: 2.290v
19: 2.314v
20: 2.338v
21: 2.362v
22: 2.386v
23: 2.410v
24: 2.434v
25: 2.458v
--------------- step 0.169
26: 2.482v
27: 2.651v
28: 2.820v
29: 2.989v
30: 3.158v
31: 3.327v
*/
#define HAL_BATMON_MIN_POLL (12 << 1)
BR
Viki Shi