This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: Is there any read-only register in CC2650 ?

Part Number: CC2650

Hello,
I am developing an application that just has to broadcast some data over the radio after a specific time interval. I want to assign distinctive Ids to each of these devices. The device will form it's ID for the first time of the boot and then query the same ID if it's rebooted anytime.
Now, I need to send some distinctive numbers along with the formed ID at the first time of the boot so that the same can be used to query the ID for subsequent reboots. For this, I need to take leverage of some kind of read-only register which contains device ID which is distinctive for every part manufactured.
Is there any such register in CC2650?

Thanks
Rahul