This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1110 433Mhz Simulation Help

Dear Sir,

I have tried to simulate the schematic of the 433MHZ Reference Design CC1110EM 2.0

the link below show the drawing in Agilent's ADS schematic.

http://picasaweb.google.com/siuchuntung/Rf?authkey=Gv1sRgCJipoK7J1viVXQ#5557449382230300978

the link below show the simulation result.

http://picasaweb.google.com/siuchuntung/Rf?authkey=Gv1sRgCJipoK7J1viVXQ#5557449383528708194

It seems that the matching is not done at the frequency of 433MHZ when I try to follow the schematic.

Would any one tell me if I have done anything wrong while I am doing the simulation?

 

Another question:

When I am doing a new design with the same PCB thickness (0.8mm) with slightly different dielectric constant (4.2 vs 4.5 used in the reference design),  can I just copy the layout from the 433MHZ CC1110EM 2.0? Do I have to change the width or height (or both) to make sure it is 50ohms and have the same angle as the reference design?

Thanks a ton!

Tony