Hi.
I am developing a wireless usb audio product using CC853x(Tx+Rx) and I have a problem with VOLUME when connected to PlayStation4.
When I connect Tx to windows 10 and adjust the volume in windows, the volume adjusted value is well received by the RX chip.
By the way, if I control the volume by operating PlayStation4 after connecting Tx to PlayStation4, only the lowest volume value is received on the RX chip.
So volume control is not available on PlayStation4. Is there a way to receive and apply the RX chip when the volume is adjusted in PlayStation4?
My settings are as follows.
TX: Standard headset
RX: Host control
Best Regards.
An.