This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RF430FRL152H: RF430FRL152H: Number of Passes Register

Part Number: RF430FRL152H
Other Parts Discussed in Thread: MSP-EXP430G2ET

Dear all,

hi my name is minhyung.

I am using RF430FRL152H and MSP-EXP430G2ET + DLP7970ABP to create a custom NFC device

The custom device which operates with NFC is to receive the LED light by the light sensor and send the data to the master kit MPS-EXP430G2ET + DLP7970ABP and send it to the PC to display it. We were going to display the data in Matlab.

I succeeded in plotting graphs in real time by receiving raw data with matlab. However I have additional problem.I want to get more than 100 data at once like GUI interface (bellow image).

I know that Number of Passes Register is number of sampling data in GUI interface. Although I modified the command to set the Number of Passes Register to 7, I can get only two data like as before. Modified command is  '01130003041802210001000410070101000000', and I received the response(bellow image).

I don't know how to get the multiple ADC data from the address that is stored the data. How can i get to know the more than 100 data at once from response?

Please reply. Thank you.

Minhyung Kang