Other Parts Discussed in Thread: MSP430F5438A-EP, MSP430F249-EP, MSP430F2274-EP, MSP430F2619S-HT
Hi,
We am looking to buy some microcontrollers which MUST have the following features:
•Low Power consumption: the lower the better
•High temperatures operation: must be at least from -55 to +125 degree C
•Wireless: It can be either built in OR the microcontroller supports 3rd party wireless device connectivity.
The microcontroller only need to handle some basic tasks, including receive data, store data in NVM, and transmit data.
We prefer microcontroller with Arm processors. If it is Arm Cortex M0+, that will be great.
Can anyone give me an suggestion to which Microcontrollers that fit my requirements?
Thanks.