Looking for Pspice Model of CC2530! Desperately needed for a senior design project!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Looking for Pspice Model of CC2530! Desperately needed for a senior design project!!
Hi Jonathan,
A full reference design (http://focus.ti.com/docs/toolsw/folders/print/cc2530em.html) is provided. For simulation purposes, the optimum load impedance (69 + j29) can be found in the data sheet (http://www.ti.com/lit/gpn/cc2530) on page 6.
Regards,
Richard.
Mr. Wallace,
Thanks for the information, The only thing is that I am using Orcad to make the pcb layout..... Is there a way to get the footprint for the TIcc2530 for orcad or is it limited to the cadstar files that were included in the package?
Thanks,
Jonathan Nylaan
Hi,
CADSTAR project files are provided and if these can not be imported or converted then it should be possible to import the gerber files instead. Some CAD programs do not allow gerber import then the gerber could be converted to DXF format and imported that way. We do not have any specific ORCAD library files for CC25xx.
Regards, Richard.