Part Number: CC2510
If we set IOCFG1.GDO_DS to 1, with VDD above 2.6V (typ 2.8-2.9) what does that do to the static current drain in PM3? (presumably there is some reason not to just always set it to 1)
Our situation is that we have a load on PIO1_1 with the processor often in PM3. The external sensor being powered through PIO1_1 is the source of the wakeup interrupt.
Sensor is usually absurdly low power (<1 uA) but briefly goes up to 20+mA (briefly = couple of microseconds). We're seeing some failures for which droop on the output of PIO1_1 is possibly the cause.