Hi,
I'm trying to use TI folded dipole antenna with CC2500 transceiver for a school project, but I have a hard time understanding the way in witch the matching was done.
In the previous posts it was said that the antenna has an impedance of about 277ohm and the chip has 80+j74ohm. The design note also specifies the traces dimensions H1, H2, H3 etc. From posts on other forums i concluded that for H1, w=0.25(trace width) and s=0.5(spacing), and for H2 and H3, w=0.5 and s=1.5, this with a dielectric substrate of 0.8mm(height).
I calculated the impedance values using TXline from AWR, assuming that the the lines are microstrip coupled lines, and the values are, for:
H1: Zodd=86ohm, Zeven=144ohm, Zdiff=2*Zodd=172
H2:Zodd=80ohm, Zeven=94ohm, Zdiff=160
The chip and antenna both have differential ports, so I'm thinking that the antenna should "see" a 277 impedance value and the transceiver should "see" a 80+j74 impedance value, but it doesen't result from calculus. Also I've considered the transmission line as a quarter wave transformer but the length is too short compered to wavelength (aprox. lambad/16) and from what i know the trace widths should be inveresed (the traces with small w and greater impedance should be connected to the antenna).
Could someone explain to me how the impedance matching is done because I want to use a dielectric substrate with a 1.6mm height and I have to recalculate the traces dimensions and it is not clear to me how. I'm knew to RF design and I'm sure something escapes me :)
Thank you, Andrei