This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530/1 SPI Example

Other Parts Discussed in Thread: CC2530, CC2531, CC2530EM, Z-STACK

I am currently developing a system which will use a CC2530 and TRF 7960 linked via SPI. As a start I'd like to confirm SPI communications between the two using evaluation boards. I have a TRF7960-CB and a SmartRF05 EB with CC2530EM and CC2531 USB Dongles. I'm taking the UART outputs from the CC2531 USB dongle, and will first confirm SPI comms on these with a scope, then connect to the 7960 and hopefully get them to play nicely. I've successfully programmed the Dongle using ExtSoC, so I can focus purely on the code.

Are there any example software designs that I can use as a base to build from, that implement SPI? I think the Z-stack code has some in, but digging through the rather massive Z-Stack code is a little daunting.


Thanks for any help,

Paul