Part Number: RF430FRL152H
Other Parts Discussed in Thread: RF430FRL154H, BQ25570
Dear TI,
Currently, I have been conducting research for my thesis project that is supposed to be COMPLETELY POWERED by RF WAVES (in short, it is a battery-less powered circuit powered from harvesting RF waves). The area I am located at has very good frequency capturing capabilities, therefore, the frequency range will be from 1MHz ~ 2.4 GHz. I kinda stumbled upon one of your devices, that is RF430FRL154H and RF430FRL152HCRGER. My question is:-
1. From the RF430FRL152HCRGER pin layout, which pin can I use to connect to the input of my circuit? Should I use the pin 24 (VDDD)?
2. Since pin 3 (VDDSW) is a switch, is it also possible to use it as a boost converter to power my circuit?
3. Is there a TI online simulation that provides services to run simulations on devices like RF430FRL152HCRGER just like the way you have WEBENCH design website to simulate Power topologies? I would really appreciate it a lot if you can also give me more insight, especially better options on how to siphon more voltage out of RF430FRL152HCRGER.
Here is a link to the 
Apart from the 3 questions above, I have been thinking of integrating an impedance matching phase for my circuit just after the antenna, but since the RF430FRL152HCRGER does not require impedance matching, can it work with any bandwidth?
My circuit has got the following specs: Vin: 0.3~5VDC, 0.7A maximum & Operating Vin: 0.8VDC