This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8531: Drill file for the demo design has errors?

Part Number: CC8531

We have sent the design files to a PCB manufacturer, but they have a problem - the drill drawing seems to be showing all of the holes the same size, but there should be a few of each of 4 bigger sizes.    I can look at the files in CADSTAR, so I wrote out the list -  A = Circle 0.6/0.3  B = QFN PAD W DRILL 0.68x1.02  C = 1.8mm Not Plated Through  D = Circle 0.4/1.3  I got these numbers from the item properties menu from the holes in question.   The board manufacturer seems to be saying that the drill file doesn't have the other diameters?  I don't know, I am not familiar with the format the drill file is in.    I am not sure how to get them what they need.  The design as it is does open in CADSTAR, but a lot of things are set up drastically different than our standard way, so  I am not able to generate a new file.

I was sent here from the tech support case

  • Hi David,

    Can you share which demo design you're referring to?

    Thanks,

    Alexis

  • oops!  I forgot to list that!

    CC85XXDK-HEADSET | User Guide:

    CC85XXDK-HEADSET | Quick Start:

  • This one has the design files -

  • Hi,

    For Audio Jack (J1 & J2) Mounting Holes. 1.7mm - 4 Holes. Please see the following Drwg.

    For Push Button Switch ( B1) - Mounting Hole Size - 1.1mm - 2 Holes. The following is the drawing.

    All others can be the same size hole.

    Yes, this is a very old design and I couldn't find the drill drawing.  But you can use the above info.

    Thanks,

    PM

  • This doesn't really help...  I can look up the parts.  I need the drill file for the PCB manufacturer fixed...  It is set up in a way that I can't do much with it, since all of the setup stuff in the CADSTAR files in this design is quite different than the setup we use.  I already sent them a list of hole sizes and the letter identifiers from the drill drawing in the design zip file, and they still couldn't build the boards.

  • Hi,

    OK. If you provide the info about the Hole Sizes and Hole Identifiers then what else your PCB Fab wants?

    Thanks,

    PM

  • Using the attached pdf-

    A = Circle 0.6/0.3

    B = QFN PAD W DRILL 0.68x1.02

    C = 1.8mm Not Plated Through

    D = Circle 0.4/1.3

    I got these numbers from the item properties menu from the pads / holes in question.

    Below is a pdf of the letter / hole locations.  And the 2 files that look like possibly the drill files that came with the original demo design.  Like I wrote, though, I am not sure since they are in an unfamiliar format.

    I tried to attach the files, but I'm getting an error from this website...

  • NCdrill.spl.txt
    %
    T1
    X046103Y057918
    X046983
    X048623Y057811
    X049773Y058478
    X050503Y058058
    X053483Y058088
    X044251Y063018
    X045623Y061148
    X045653Y060378
    X046213Y061284
    X046253Y060738
    X046283Y059168
    X047103Y060858
    X047243Y062088
    X047557Y062298
    X047577Y063508
    X047603Y058798
    X047613Y060668
    X047663Y062628
    X047673Y060988
    X047713Y063218
    X048063Y062988
    X04808Y060195
    Y059597
    X048313Y063738
    Y063448
    X048379Y059298
    Y059896
    X048413Y061208
    X048678Y060195
    Y059597
    X048703Y061188
    X048763Y062892
    X048973Y061101
    X048977Y059896
    Y059298
    X049243Y061028
    X049523Y060988
    X049803Y059168
    X049823Y058808
    X049923Y061858
    X050153Y060418
    X050313Y063348
    X050743Y063678
    X051273Y063068
    X051343Y062418
    X053743Y059908
    X042683Y064908
    X044224Y065998
    X044803Y065798
    X045093Y065078
    X045783Y066108
    X045893Y065608
    X046823Y065898
    Y065548
    X047013Y063888
    X047252Y065808
    X047499Y065598
    X047533Y064698
    X047693Y065798
    X047885Y065588
    X048083Y065828
    X048223Y065548
    X048303Y064728
    X048663Y064988
    X048733Y065818
    X048943Y065198
    X049023Y065788
    X049303Y066208
    X049313Y065238
    X049573Y066018
    X050055Y065008
    X050243Y066068
    X050293Y065378
    X050363Y063898
    X050733Y064958
    X051333Y065998
    X05134Y064638
    X051513Y066208
    X052333Y065118
    X052933Y065358
    X053133Y064288
    X053943Y066248
    X043243Y068568
    X043663Y067898
    X043703Y067478
    X044093Y068738
    X044793Y067798
    X044853Y068138
    X045233Y068798
    X045263Y068478
    X045333Y066778
    X045453Y068138
    X045463Y067798
    X045473Y067458
    X04635Y068808
    X046483Y067025
    X046904Y068468
    X047511Y067999
    Y067093
    Y066641
    Y067546
    X047962Y067095
    X047964Y067546
    Y066641
    Y067999
    X048063Y068788
    X048416Y067546
    Y066641
    Y067999
    Y067093
    X048869Y067999
    Y066641
    Y067093
    Y067546
    X049803Y068398
    X049824Y066375
    X050083Y067408
    X050253Y068618
    X050603Y067688
    X050623Y066508
    X050763Y068368
    X051343Y068248
    X051543Y068668
    X051763Y068268
    X051983Y068638
    X052213Y068268
    X052293Y066398
    X052823Y068038
    X054033Y066548
    X054613
    X04322Y069328
    X043913Y070708
    X044123Y071218
    X044833Y069408
    X045523Y070708
    X045683Y070118
    X045703Y070478
    X046083Y071008
    X046223Y070068
    X046273Y070378
    X046623Y071168
    X047163Y071208
    X047193Y070198
    X047423Y069758
    X047673Y069618
    X047997Y071001
    Y070434
    X04828Y070717
    X048564Y070434
    Y071001
    X048923Y071338
    X048963Y069758
    X049223Y069071
    X049323Y070888
    X049523Y071438
    X049533Y070688
    X049573Y070378
    X049713Y069678
    X050198Y070666
    X050203Y071438
    X050863Y069968
    X051113Y069828
    X051143Y070588
    X051202Y071316
    X051533Y070788
    X052233Y068898
    X054973Y071298
    X042653Y073638
    Y072368
    Y072848
    X042893Y073088
    Y073988
    X043143Y072738
    X043273Y073658
    X043353Y073188
    Y072368
    X043653Y072498
    X043683Y073988
    X043993Y073658
    X044133Y071718
    X044363Y073158
    X044463Y073988
    X044713Y073658
    X045073Y073458
    X045303Y072828
    X045323Y073988
    X045673Y073658
    X045703Y072748
    X046043Y073988
    X046103Y072348
    X046163Y072718
    X046643Y073208
    Y073988
    X046813Y071718
    X046893Y072818
    X046943Y073208
    X047103Y073838
    X047173Y072978
    X047273Y073268
    X047343Y072738
    X047593Y072988
    Y073838
    Y073358
    X047733Y071718
    X048763Y072818
    Y073428
    Y073868
    X049023Y072698
    X049243Y073318
    X049513Y072408
    X049603Y073798
    X049923Y073498
    X050073Y072728
    X050183Y072388
    X050203Y071868
    X050233Y073168
    X050273Y073798
    X050553Y072728
    X050713Y073498
    X050763Y072428
    X050983Y072118
    X051023Y071588
    X051053Y072848
    X051133Y073168
    X051193Y073798
    X051303Y072428
    X051533Y073498
    X051893Y073798
    X051953Y072578
    X052023Y073168
    X052343Y073498
    X052673Y073168
    X052713Y073798
    X052823Y072718
    X053113Y073798
    Y073318
    X053543Y072958
    X054123Y072058
    Y072878
    X054603Y071748
    Y072648
    X054973Y073668
    Y072088
    Y072878
    X042653Y074408
    X043313
    X044133
    X044923
    X045723
    X046353
    X046913Y074218
    X047303Y074198
    X048763Y074408
    X048983Y074198
    X049273Y074098
    X049553Y074408
    X049893Y074098
    X050343Y074408
    X050753Y074098
    X051133Y074408
    X051553Y074098
    X051923Y074408
    X052333Y074098
    X052713Y074408
    X053083Y074098
    X053503Y074408
    X053923Y074118
    X054293Y074408
    X054603Y074118
    X054973Y074408
    T2
    X049023Y063604
    X049559
    X049023Y064407
    X049291Y064006
    X049559Y064407
    T3
    X044644Y058942
    X052724Y058932
    Y061688
    X044644Y061698
    M30
    

  • drill.spl.txt
    G70*
    %FSLAX24Y24*%
    %ADD11C,0.0010*%
    %AMUSER12*
    1, 1, 0.0276, 0.0, 0.0*
    1, 0, 0.0138, 0.0, 0.0*%
    %ADD12USER12*%
    %ADD13C,0.0051*%
    D11*
    X42403Y57548D02*
    X42403Y77858D01*
    X55233Y77858*
    X55233Y57548*
    X42403Y57548*
    D12*
    X48080Y60195D03*
    X48080Y59597D03*
    X48379Y59896D03*
    X48379Y59298D03*
    X48678Y60195D03*
    X48678Y59597D03*
    X48977Y59896D03*
    X48977Y59298D03*
    X54607Y68309D03*
    D13*
    X54406Y68109D02*
    X54406Y68192*
    X54406Y68510D01*
    X54406Y68293D02*
    X54423Y68293D01*
    X54573Y68393*
    X54423Y68293D02*
    X54573Y68192D01*
    D12*
    X54607Y64766D03*
    D13*
    X54406Y64565D02*
    X54406Y64649*
    X54406Y64967D01*
    X54406Y64749D02*
    X54423Y64749D01*
    X54573Y64850*
    X54423Y64749D02*
    X54573Y64649D01*
    D12*
    X47997Y70434D03*
    X47997Y71001D03*
    X48280Y70717D03*
    X48564Y70434D03*
    X48564Y71001D03*
    X44644Y58942D03*
    D13*
    X44444Y58741D02*
    X44711Y58859*
    X44678Y58825D01*
    X44477Y58825*
    X44444Y58859*
    X44444Y59110*
    X44477Y59143*
    X44678Y59143*
    X44711Y59110*
    D12*
    X44644Y61698D03*
    D13*
    X44444Y61497D02*
    X44711Y61614*
    X44678Y61581D01*
    X44477Y61581*
    X44444Y61614*
    X44444Y61865*
    X44477Y61899*
    X44678Y61899*
    X44711Y61865*
    D12*
    X52724Y58932D03*
    D13*
    X52524Y58731D02*
    X52791Y58849*
    X52758Y58815D01*
    X52557Y58815*
    X52524Y58849*
    X52524Y59100*
    X52557Y59133*
    X52758Y59133*
    X52791Y59100*
    D12*
    X52724Y61688D03*
    D13*
    X52524Y61487D02*
    X52791Y61604*
    X52758Y61571D01*
    X52557Y61571*
    X52524Y61604*
    X52524Y61855*
    X52557Y61889*
    X52758Y61889*
    X52791Y61855*
    D12*
    X49559Y63604D03*
    D13*
    X49358Y63403D02*
    X49358Y63487*
    X49492Y63805D01*
    X49626Y63487*
    X49408Y63604D02*
    X49575Y63604D01*
    D12*
    X49559Y64407D03*
    D13*
    X49358Y64206D02*
    X49358Y64290*
    X49492Y64608D01*
    X49626Y64290*
    X49408Y64407D02*
    X49575Y64407D01*
    D12*
    X49291Y64006D03*
    D13*
    X49090Y63805D02*
    X49090Y63888*
    X49224Y64206D01*
    X49358Y63888*
    X49140Y64006D02*
    X49308Y64006D01*
    D12*
    X49023Y63604D03*
    D13*
    X48823Y63403D02*
    X48823Y63487*
    X48956Y63805D01*
    X49090Y63487*
    X48873Y63604D02*
    X49040Y63604D01*
    D12*
    X49023Y64407D03*
    D13*
    X48823Y64206D02*
    X48823Y64290*
    X48956Y64608D01*
    X49090Y64290*
    X48873Y64407D02*
    X49040Y64407D01*
    D12*
    X48869Y66641D03*
    X48416Y66641D03*
    X47964Y66641D03*
    X47511Y66641D03*
    X47511Y67093D03*
    X47962Y67095D03*
    X48416Y67093D03*
    X48869Y67093D03*
    X48869Y67546D03*
    X48416Y67546D03*
    X47964Y67546D03*
    X47511Y67546D03*
    X47511Y67999D03*
    X47964Y67999D03*
    X48416Y67999D03*
    X48869Y67999D03*
    X52933Y65358D03*
    X45463Y67798D03*
    X44793Y67798D03*
    X49533Y70688D03*
    X48223Y65548D03*
    X44133Y71718D03*
    X48083Y65828D03*
    X44123Y71218D03*
    X52333Y65118D03*
    X44251Y63018D03*
    X47252Y65808D03*
    X44803Y65798D03*
    X45093Y65078D03*
    X47499Y65598D03*
    X53743Y59908D03*
    X49823Y58808D03*
    X53133Y64288D03*
    X45473Y67458D03*
    X46083Y71008D03*
    X49573Y66018D03*
    X47885Y65588D03*
    X43913Y70708D03*
    X47613Y60668D03*
    X46283Y59168D03*
    X49923Y61858D03*
    X48733Y65818D03*
    X51113Y69828D03*
    X51533Y70788D03*
    X51343Y68248D03*
    X48413Y61208D03*
    X49523Y60988D03*
    X52213Y68268D03*
    X49243Y61028D03*
    X51983Y68638D03*
    X51763Y68268D03*
    X48973Y61101D03*
    X49573Y70378D03*
    X44853Y68138D03*
    X48703Y61188D03*
    X51543Y68668D03*
    X52823Y68038D03*
    X48313Y63738D03*
    X45523Y70708D03*
    X51202Y71316D03*
    X45453Y68138D03*
    X45653Y60378D03*
    X43663Y67898D03*
    X50983Y72118D03*
    X43653Y72498D03*
    X45303Y72828D03*
    X49223Y69071D03*
    X47713Y63218D03*
    X43703Y67478D03*
    X49023Y72698D03*
    X51143Y70588D03*
    X45263Y68478D03*
    X45623Y61148D03*
    X51023Y71588D03*
    X45703Y70478D03*
    X49323Y70888D03*
    X50198Y70666D03*
    X49824Y66375D03*
    X48063Y68788D03*
    X47243Y62088D03*
    X50153Y60418D03*
    X50243Y66068D03*
    X49773Y58478D03*
    X46483Y67025D03*
    X43220Y69328D03*
    X46983Y57918D03*
    X46823Y65898D03*
    X48623Y57811D03*
    X53483Y58088D03*
    X50503Y58058D03*
    X48763Y62892D03*
    X47663Y62628D03*
    X47423Y69758D03*
    X48063Y62988D03*
    X50733Y64958D03*
    X51273Y63068D03*
    X51333Y65998D03*
    X49023Y65788D03*
    X52293Y66398D03*
    X48663Y64988D03*
    X44093Y68738D03*
    X47693Y65798D03*
    X49303Y66208D03*
    X51513Y66208D03*
    X48943Y65198D03*
    X54033Y66548D03*
    X54613Y66548D03*
    X48313Y63448D03*
    X49313Y65238D03*
    X51133Y74408D03*
    X46223Y70068D03*
    X46273Y70378D03*
    X44133Y74408D03*
    X50083Y67408D03*
    X44923Y74408D03*
    X53943Y66248D03*
    X45723Y74408D03*
    X46643Y73208D03*
    X47343Y72738D03*
    X47593Y72988D03*
    X43683Y73988D03*
    X47533Y64698D03*
    X47733Y71718D03*
    X47193Y70198D03*
    X48983Y74198D03*
    X46103Y57918D03*
    X44713Y73658D03*
    X47103Y60858D03*
    X44363Y73158D03*
    X47603Y58798D03*
    X46163Y72718D03*
    X51553Y74098D03*
    X46353Y74408D03*
    X50363Y63898D03*
    X46043Y73988D03*
    X45673Y73658D03*
    X42893Y73988D03*
    X43353Y73188D03*
    X44224Y65998D03*
    X43273Y73658D03*
    X47163Y71208D03*
    X54123Y72878D03*
    X52233Y68898D03*
    X49523Y71438D03*
    X47593Y73838D03*
    X46913Y74218D03*
    X47303Y74198D03*
    X47273Y73268D03*
    X43143Y72738D03*
    X49553Y74408D03*
    X50313Y63348D03*
    X47593Y73358D03*
    X49243Y73318D03*
    X49603Y73798D03*
    X46253Y60738D03*
    X50273Y73798D03*
    X51053Y72848D03*
    X53083Y74098D03*
    X43353Y72368D03*
    X51340Y64638D03*
    X46350Y68808D03*
    X54973Y71298D03*
    X54603Y71748D03*
    X50623Y66508D03*
    X54973Y72088D03*
    X54603Y72648D03*
    X49923Y73498D03*
    X54973Y73668D03*
    X53503Y74408D03*
    X54973Y74408D03*
    X54973Y72878D03*
    X49803Y59168D03*
    X53923Y74118D03*
    X53113Y73798D03*
    X54293Y74408D03*
    X53543Y72958D03*
    X47673Y69618D03*
    X50763Y68368D03*
    X44833Y69408D03*
    X54603Y74118D03*
    X46623Y71168D03*
    X50713Y73498D03*
    X51533Y73498D03*
    X51193Y73798D03*
    X46904Y68468D03*
    X48763Y74408D03*
    X45893Y65608D03*
    X47013Y63888D03*
    X49893Y74098D03*
    X49513Y72408D03*
    X50343Y74408D03*
    X51923Y74408D03*
    X49273Y74098D03*
    X50753Y74098D03*
    X51893Y73798D03*
    X48763Y73428D03*
    X50253Y68618D03*
    X52333Y74098D03*
    X50203Y71868D03*
    X50763Y72428D03*
    X43313Y74408D03*
    X48763Y72818D03*
    X50203Y71438D03*
    X50183Y72388D03*
    X53113Y73318D03*
    X48763Y73868D03*
    X50553Y72728D03*
    X42653Y72848D03*
    X50073Y72728D03*
    X51303Y72428D03*
    X54123Y72058D03*
    X52343Y73498D03*
    X46893Y72818D03*
    X47103Y73838D03*
    X52673Y73168D03*
    X42653Y74408D03*
    X42653Y72368D03*
    X52713Y74408D03*
    X42653Y73638D03*
    X50233Y73168D03*
    X47557Y62298D03*
    X49803Y68398D03*
    X45783Y66108D03*
    X46643Y73988D03*
    X51133Y73168D03*
    X46823Y65548D03*
    X52713Y73798D03*
    X48923Y71338D03*
    X45323Y73988D03*
    X43993Y73658D03*
    X51343Y62418D03*
    X46813Y71718D03*
    X45333Y66778D03*
    X51953Y72578D03*
    X43243Y68568D03*
    X46103Y72348D03*
    X44463Y73988D03*
    X45073Y73458D03*
    X48963Y69758D03*
    X45703Y72748D03*
    X50863Y69968D03*
    X47673Y60988D03*
    X46943Y73208D03*
    X49713Y69678D03*
    X48303Y64728D03*
    X47173Y72978D03*
    X47577Y63508D03*
    X42683Y64908D03*
    X50603Y67688D03*
    X46213Y61284D03*
    X42893Y73088D03*
    X45683Y70118D03*
    X50055Y65008D03*
    X52823Y72718D03*
    X45233Y68798D03*
    X50293Y65378D03*
    X50743Y63678D03*
    X52023Y73168D03*
    M02*
    

  • Hi,

    Drill.spl and NCDrill.spl are Gerber files.

    They can open these files by using Gerber viewer.

    Thanks,

    PM

  • I figured that one or the other was. 

    The  Drill.spl opens in a gerber viewer.  It shows an image of the hole positions.  It seems to have some indication on the relatively few holes that have different sizes. 

    NCDrill.spl I can only view with a text editor, it is unrecognized by the Gerber viewer I use.   It displays as a cryptic list of mostly numbers.  Nothing I can "read" to figure out if it is correct or wrong.

    The PCB manufacturer is saying that the holes are all the same size /  the data for the different diameters isn't in the file.   I have no way to check. 

    I have no way to generate a new file - Short of piece by piece re-drawing the schematic, building any part I don't have in my library, and laying out the PCB myself.  I will have to do this eventually, but we were hoping to at least get the demo design up and running before spending this time.

  • NOTE - I re sent these 2 files to the PCB manufacturer.  They report that all of the hole diameters are the same size.

  • I notice a flag "TI thinks this is resolved".

    It is NOT resolved.  I still do not have a usable drill file for this design. 

  • Hi,

    Attached are the Drill Hole Sizes.

    You can see the Drill Legend in PDF and also in Gerber Files (Drill.spl). Both are attached for your ready reference.

    We usually provide Drill Drawing ( Drill Legend with hole sizes) in PDF to PCB Fab along with Drill file and NC Drill file. This should be enough for drilling the holes on to the PCB by PCB Fab.

    2438.DrillHoleSizes.txt
    ************************************ ROW 6 ************************************
    
    
     [<None>] :: [Drill Drawing] :: [drill.col] :: [Photo Plotter] :: [ext_gerber.usr] :: [Photoplot_art.sel] :: [drill.spl] 
    
    ~~~~~~~~~~~~~~~~~~~ Warning ~~~~~~~~~~~~~~~~~~~~
    
    The following items are displayed:
        Component Areas
    
    ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
    
    Drill Report
    ------------
    
          Size    Length    Plate Through    Letter     Count
          ----    ------    -------------    ------     -----
         0.300     0.000              Yes         @       271
         0.450     0.000              Yes         A         5
         1.300     0.000               No         k         2
        1.8034     0.000              Yes         C         4
    
    
    Symbol Availability Report
    --------------------------
    
    Position    Shape          Usage           Size    Orient        Length     Count
    --------    -----          -----           ----    ------        ------     -----
    
    Predefined Symbols
    ------------------
    
    
    Auto Allocated Symbols
    ----------------------
    
    11          CIRCLE         Drawn         0.0254                                  
    12          ANNULUS        Flashed        0.700                   0.350       282
    13          CIRCLE         Drawn          0.130                                  
    
    
    Row 6 completed successfully.

    5153.CC85XX headset reference design 1_3_LAYOUT.pdf

    5852.drill.spl

    2047.NCdrill.spl

    Thanks,

    PM

  • Hi,

    Attached are the Drill Hole Sizes.

    You can see the Drill Legend in PDF and also in Gerber Files (Drill.spl). Both are attached for your ready reference.

    We usually provide Drill Drawing ( Drill Legend with hole sizes) in PDF to PCB Fab along with Drill file and NC Drill file. This should be enough for drilling the holes on to the PCB by PCB Fab.

    5141.DrillHoleSizes.txt
    ************************************ ROW 6 ************************************
    
    
     [<None>] :: [Drill Drawing] :: [drill.col] :: [Photo Plotter] :: [ext_gerber.usr] :: [Photoplot_art.sel] :: [drill.spl] 
    
    ~~~~~~~~~~~~~~~~~~~ Warning ~~~~~~~~~~~~~~~~~~~~
    
    The following items are displayed:
        Component Areas
    
    ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
    
    Drill Report
    ------------
    
          Size    Length    Plate Through    Letter     Count
          ----    ------    -------------    ------     -----
         0.300     0.000              Yes         @       271
         0.450     0.000              Yes         A         5
         1.300     0.000               No         k         2
        1.8034     0.000              Yes         C         4
    
    
    Symbol Availability Report
    --------------------------
    
    Position    Shape          Usage           Size    Orient        Length     Count
    --------    -----          -----           ----    ------        ------     -----
    
    Predefined Symbols
    ------------------
    
    
    Auto Allocated Symbols
    ----------------------
    
    11          CIRCLE         Drawn         0.0254                                  
    12          ANNULUS        Flashed        0.700                   0.350       282
    13          CIRCLE         Drawn          0.130                                  
    
    
    Row 6 completed successfully.

    3771.CC85XX headset reference design 1_3_LAYOUT.pdf

    2845.drill.spl

    4667.NCdrill.spl

    Thanks,

    PM

  • Thank you,  I will send these to them.

    Dave