Other Parts Discussed in Thread: MSP430G2553, , MSP430F5529
Tool/software: Code Composer Studio
Hello,
I want to using the RF430FRL152H & TRF7970ABP+MSP430G2553 to measure the analog signal. I want to implement the following functions:
(1)The ADC in RF430FRL152H samples the analog signal at a sampling frequency of 20Hz~25Hz;
(2)TRF7970ABP+MSP430G2553 obtains signal through RF field and sends it to PC through serial port for real-time and continuous acquisition.
So, there is the code I programmed in RF430FRL152H
-------------------------------------------------------CODE SPACE----------------------------------------------------------------------------
#include <rf430frl152h.h>
#include <string.h>
#include "types.h"
//*****************************FUNCTION PROTOTYPES********************************/
void DeviceInit(void);
void initISO15693(u16_t parameters );
void SetupSD14(unsigned char channel);
//********************************************************************************/
u16_t SamplesBuffer[4];
//u08_t State;
//enum state_type
//{
// IDLE_STATE = 1,
// ONE_SHOT_TEMP_REFERENCE_SAMPLE_STATE = 2,
// ONE_SHOT_TEMP_THERMISTOR_SAMPLE_STATE = 3,
//};
enum Channel_Types
{
ADC0_CHANNEL = 0x0,
INTERNAL_TEMPERATURE_CHANNEL = 0x1,
THERMISTOR_ADC2_CHANNEL = 0x2,
REFERENCE_ADC1_CHANNEL = 0x3,
};
//*****************************DEFINES *******************************************/
#define CLEAR_BLOCK_LOCKS BIT3
#define FRAM_LOCK_BLOCK_AREA_SIZE 38
#define FRAM_LOCK_BLOCKS 0xF840 //Address of ISO15693 lock blocks
#define ROM_EUSCI_SUPPORT_ENABLED BIT2
#define EROM_EUSCI_SUPPORT_DISABLED 0
#define ROM_SENSOR_SUPPORT_ENABLED BIT7
#define ROM_SENSOR_SUPPORT_DISABLED 0
#define NFC_BRIDGE_DISABLED BIT6
#define NFC_BRIDGE_ENABLED 0
#define EIGHT_BYTE_BLOCK BIT0
#define FOUR_BYTE_BLOCK 0
#define FIRST_ISO_PAGE BIT1
#define SECOND_ISO_PAGE 0
/* Firmware System Control Byte
*
* Bit 0: ISOBlockSize 0 - 4 byte, 1 - 8 byte
* Bit 1: Page 0 - page 1, 1 - page 0 (Effective only for 4-byte block mode)
* Bit 2: ROMEUSCISupportEnabled 0 - disabled, 1 - enabled (Forced to 0 on RF430FRL153H)
* Bit 3-5: ReservedISO
* Bit 6: NFCBridgeDisable 0 - enabled, 1 - disabled (see note below)
* Bit 7: ROMSensorSupportEnable 0 - disabled, 1 - enabled (Forced to 0 on RF430FRL154H)
*
* NFC bridge is recommended to be disabled in this project. Unexpected behaviour can occur,
* trying to use it, due to the configuration being setup here.
*
* If eUSCI host controller portion is needed along with the RF functionality, the default project
* must be used. That is NFC cannot be supported in that application (because the I2C/SPI host controller
* control registers are in the same place that the NFC file needs to be). However the rest of the FRAM
* memory can be used for storing and reading using ISO15693.
*/
#define FIRMWARE_CONTROL_ADDRESS 0xF867
#pragma RETAIN(Firmware_System_Control_Byte);
#pragma location = FIRMWARE_CONTROL_ADDRESS
const u08_t Firmware_System_Control_Byte = ROM_SENSOR_SUPPORT_DISABLED + EROM_EUSCI_SUPPORT_DISABLED + NFC_BRIDGE_DISABLED + FOUR_BYTE_BLOCK + FIRST_ISO_PAGE; //0x7F, // this value sets the firmware system control register
// ROM variables - DO NOT CHANGE !!!
// Declared to protect from use by compiler
/********************************************/
#pragma RETAIN(DS)
#pragma location = 0x1C00
u08_t DS;
#pragma RETAIN(RF)
#pragma location = 0x1C6A
const u08_t RF;
#pragma RETAIN(NRX)
#pragma location = 0x1CA4 //rx
const u08_t NRX[34];
#pragma RETAIN(NTX)
#pragma location = 0x1CC6 //tx
const u08_t NTX[33];
#pragma RETAIN(EL)
#pragma location = 0x1CF2
const u08_t EL;
#pragma RETAIN(PF)
#pragma location = 0x1C0A
const u16_t PF[48];
/********************************************/
#define NDEF_START_ADDRESS 0xF868
#pragma RETAIN(NFC_NDEF_Message);
#pragma location = NDEF_START_ADDRESS; // the location of the address
const u08_t NFC_NDEF_Message[21] = {
// Most of the Android applications will not recognize this message as NDEF at this point, due to the
// tag not being registered with Android NFC stack. However ISO15693 RFID communication is supported.
// Block 0
0xE1, // NDEF Magic Number
0x40, // Version Number, read/write access conditions
0xF2,//F3*4/8 = 0x79 //0x7E, // 1008 bytes / 8 = 126 blocks
0x00,//extended memory //0x00, // does not support read multiple blocks (limited to only 3 blocks)
// Block 1
0x03, // NDEF Message present
0x0B, // Length , 11 bytes
0xD1, // Record header
0x01, // type length
// Block 2
0x07, // Payload length
0x55, // Record Type U (URI)
0x01, // URI header identifier
0x74, // 't'
// Block 3
0x69, // 'i'
0x2E, // '.'
0x63, // 'c'
0x6F, // 'o'
// Block 4
0x6D, // 'm'
0xFE, // TLV terminator
0x00, // Empty don't care
0x00, // Empty don't care
};
/*********************** SUMMARY **************************************************************************************************
* This project only utilizes the RF stack (ISO15693) on the ROM of the RF430FRL15xH. This setup allows the user to make a
* custom application that is run from FRAM. Only the RF13M vector that runs the RF stack needs to be pointing to its
* ROM location.
*/
/**************************************************************************************************************************************************
* Main
***************************************************************************************************************************************************
*
* Brief :
*
* Param[in] : None
*
*
* Param[out]: None
*
* Return :
*
**************************************************************************************************************************************************/
void main()
{
WDTCTL = WDTPW + WDTHOLD; // Stop watchdog
// ROM RF13M module setup ** The following three lines are needed for proper RF stack operation
DS = 1; // ROM variable needs to be initialized here
asm ( " CALL #0x5CDA "); // Call ROM function ( Initialize function pointers)
asm ( " CALL #0x5CAC "); // Call ROM function ( Check part configuration)
initISO15693(CLEAR_BLOCK_LOCKS);
DeviceInit();
while(1)
{
//State = ONE_SHOT_TEMP_REFERENCE_SAMPLE_STATE;
SetupSD14(ADC0_CHANNEL);
}
//__bis_SR_register(LPM3_bits + GIE); // sampling here two channels, SD14_ADC will wake up twice and store the conversions
// into samplesBuffer, last conversion will cause this LPM mode to be exited and continue to below.
//processing can be done on the stored conversions here
// SamplesBuffer[0] = ADC0 conversion result
__bis_SR_register(LPM3_bits + GIE);
__no_operation();
}
/* SetupSD14 *
* The channel to be sampled (thermistor or reference resistor) *
* Function: This function is setup for sampling either a thermistor or a reference resistor */
void SetupSD14(unsigned char channel)
{
// setting: channel to be sampled, the programmable amplifier gain (2x), CIC filter, SD14INTDLY0 needed since CIC filter needs atleast two consecutive samples before producing an accurate result
// SDRATE at fastest result possible but also not the most accurate, also enabled is the SD14RBEN which is the current source into the thermistor and references resistor
SD14CTL1 = SD14GAIN_0 + SD14FILT__CIC + SD14RATE__CIC32 + SD14INTDLY_0 + channel;
// clock from ACLK (64kHz from VLO clock), SD14DIV1 is set for divide by 32 times (SD14 needs a 2kHz clock),
SD14CTL0 = SD14IE + SD14DIV1; // 2 kHz sampling rate, ACLK source, SVSS ground (.125V), interrupt enable
SD14CTL0 |= SD14EN; // SD14 module enabled,
SD14CTL0 |= SD14SC; // start the conversion
}
//Set and Read ADC0
#pragma vector=SD_ADC_VECTOR
interrupt void SD14_ADC (void)
{
switch(__even_in_range(SD14IV,4)) //SD14IV register status:00h-no interrupt pending; 02h-SD14MEM overflow(SD14OVIFG);04h-SD14MEM new result(SD14IFG)
{
case SD14IV__NONE: // no interrupt pending
break;
case SD14IV__OV: //SD14MEM overflow - SD14OVIFG
SD14CTL0 &= ~SD14OVIFG; // clear the overflow bit
break;
case SD14IV__RES:
SD14CTL0 &= ~SD14IFG; // clear the data available interrupt
SamplesBuffer[0] = SD14MEM0;
SD14CTL0 |= SD14EN + SD14SC;
/*if (State == ONE_SHOT_TEMP_REFERENCE_SAMPLE_STATE)
{
State = ONE_SHOT_TEMP_THERMISTOR_SAMPLE_STATE;
SamplesBuffer[0] = SD14MEM0; // compensation for thermistor current bias error
SetupSD14(THERMISTOR_ADC2_CHANNEL); //setup ADC and start the conversion
}
else if (State == ONE_SHOT_TEMP_THERMISTOR_SAMPLE_STATE)
{
SamplesBuffer[1] = SD14MEM0; // compensation for thermistor current bias error
SD14CTL0 &= ~SD14EN; //disable the SD14 until it is restarted if using consecutive readings by the timer
State = IDLE_STATE;
//conversion completed, data available
__bic_SR_register_on_exit(LPM4_bits); //exit LPM mode after this interrupt
}*/
break;
}
}
/**************************************************************************************************************************************************
* DeviceInit
***************************************************************************************************************************************************
*
* Brief : Initialize the clock system and other settings
* Patchable function
*
* Param[in] : parameters: has these independent options
* INITIALIZE_DEVICE_CLOCK_SYSTEM - initializes the clock system
* POPULATE_INTERRUPT_VECTOR_IN_INITIALIZATION - populate the default interrupt vectors and recalculate their CRC
*
* Param[out]: None
*
* Return None
*
* Patchable : Yes
**************************************************************************************************************************************************/
void DeviceInit(void)
{
P1SEL0 = 0xF0; //keep JTAG
P1SEL1 = 0xF0; //keep JTAG
P1DIR &= ~0xEF;
P1REN = 0;
CCSCTL0 = CCSKEY; // Unlock CCS
CCSCTL1 = 0; // do not half the clock speed
CCSCTL4 = SELA_1 + SELM_0 + SELS_0; // Select VLO for ACLK and select HFCLK/DCO for MCLK, and SMCLK
CCSCTL5 = DIVA_2 + DIVM_1 + DIVS_1; // Set the Dividers for ACLK (4), MCLK, and SMCLK to 1
CCSCTL6 = XTOFF; // Turns of the crystal if it is not being used
CCSCTL8 = ACLKREQEN + MCLKREQEN + SMCLKREQEN; //disable clocks if they are not being used
CCSCTL0_H |= 0xFF; // Lock CCS
return;
}
/**************************************************************************************************************************************************
* initISO15693
***************************************************************************************************************************************************
*
* Brief : Initializes the RF Stack
*
* Param[in] : parameter - the configuration to setup the ISO15693 (option to clear the lock blocks)
*
* Param[out]: None
*
* Return None
**************************************************************************************************************************************************/
void initISO15693(u16_t parameters )
{
// enable interrupts ** Do not change the following two lines, needed for proper RF stack operatoin
RF13MCTL |= RF13MTXEN + RF13MRXEN + RF13MRFTOEN; // set up rx and tx functionality on RF13M module
RF13MINT |= RF13MRXIE + RX13MRFTOIE; // enable interrupts on RX and on timeout and over and under flow checking
if (parameters & CLEAR_BLOCK_LOCKS )
{
//initializeBlockLocks(); //inline function
memset ((u08_t *) FRAM_LOCK_BLOCKS, 0xFF, FRAM_LOCK_BLOCK_AREA_SIZE); //block is locked with a zero bit, clears FRAM and RAM lock blocks
}
}
//#pragma vector = RFPMM_VECTOR
//__interrupt void RFPMM_ISR(void)
//{
//}
//
//#pragma vector = PORT1_VECTOR
//__interrupt void PORT1_ISR(void)
//{
//}
//
//#pragma vector = SD_ADC_VECTOR
//__interrupt void SD_ADC_ISR(void)
//{
//}
//
//#pragma vector = USCI_B0_VECTOR
//__interrupt void USCI_B0_ISR(void)
//{
//}
//#pragma CODE_SECTION(RF13M_ISR, ".fram_driver_code") // comment this line for using ROM's RF13M ISR, uncomment next one, see .cmd file for details
#pragma CODE_SECTION(RF13M_ISR, ".rf13m_rom_isr") // comment this line for creating a custom RF13M ISR that will exist in FRAM, bypassing ROM's, uncomment previous
#pragma vector = RF13M_VECTOR
__interrupt void RF13M_ISR(void)
{
// Right now this vector is pointing to the ROMs firmware location that runs the RF stack.
// Entering code here will, without changing the CODE_SECTION lines
// above, will cause an error.
// Changing the code section above will cause the ROM RF stack to be bypassed. New handler will need to be created.
}
//#pragma vector = WDT_VECTOR
//__interrupt void WDT_ISR(void)
//{
//}
//
//#pragma vector = TIMER0_A1_VECTOR
//__interrupt void TimerA1_ISR(void)
//{
//}
//
//#pragma vector = TIMER0_A0_VECTOR
//__interrupt void TimerA0_ISR(void)
//{
//}
//
//#pragma vector = UNMI_VECTOR
//__interrupt void UNMI_ISR(void)
//{
//}
//
//#pragma vector = SYSNMI_VECTOR
//__interrupt void SysNMI_ISR(void)
//{
//}
---------------------------------------------------CODE SPACE----------------------------------------------------------------
I have those question
(1)Is my code correct, why can't I achieve continuous and uninterrupted data collection?
(2)Is my ADC set correctly? Can I use some serial assistants to get the data?