Part Number: CC8530
RX Test with PurePath Wireless Commander gives an error. Attach the problem as an image file Upnida. How can I solve the problem?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From the PurePath Commander help documents:
Perform an RF test with a continuous or modulated signal. Frequency, TX power, number of samples and RSSI threshold is configurable. The receiver measures the RSSI value. The RSSI value shown is the average after the 5 lowest and 5 highest samples have been removed. The test passed if the average is above the given RSSI threshold.
There are three ways of running an RF test:
I bolded the relevant bullet point for your test. How are you providing stimuli for the device to receive?