Other Parts Discussed in Thread: RF430FRL152H, MSP430G2553
Tool/software: Code Composer Studio
Hi,
I am now using the TRF7970ABP+MSP430G2553 read DATA from rf430frl152h, the frequency of sensor is 25Hz. But now it takes too long to send the read command from the PC host to the PC receiving the data~80ms, so the data cannot be displayed on the PC in real time at a frequency of 25Hz. So what should I do?
I also want to shorten the whole process to 5ms to meet the requirement of faster sampling frequency(~200Hz), is there a possibility of realization?
Best Regards,
Senhao Zhang