This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
I want to read the UID of my trasponder(which using ISO15693) with TRF7970A(boosterpack dlp-7970abp) with the Wipy(ESP32,Power Supply 3.3V). Let me show the instructions which I did:
1.Enable
2.Software inizialization (0x83)
3. Idle (0x80)
After 1. 2. 3. I can read all register like in page 52 of datasheet
4.Single write of 0x00 in Modulator Control
5.Single Read of Modulator Control
6.Check External RF,0x99(0x19)
7.Read Single of RSSI levels(0x0f)(read 0x40)
8.Write Continuous from CHIP STATUS CONTROL to REGULATOR CONTROL:
Chip status control: 0x01
Iso control : 0x02
ISO_14443B_OPTIONS:0x0a
ISO_14443A_OPTIONS:0x40
TX_TIMER_EPC_HIGH:0x0b
TX_TIMER_EPC_LOW 0x00
TX_PULSE_LENGTH_CONTROL 0x14
RX_NO_RESPONSE_WAIT_TIME 0x0f
RX_WAIT_TIME 0x18
MODULATOR_CONTROL 0x00
RX_SPECIAL_SETTINGS 0x4c
REGULATOR_CONTROL 0x00.
Is this correct configuration?
6.Inventory Command: 0x8f,0x91,0x3d,0x00,0x300x26,0x01,0x00
7. Dummy read of ragister IRQ(0x80)----->First interrupt
But the second Interrupt when I put the trasponder doesn't occur. Why?
Which is the problem?
Thanks a lot
I'll very appreciate your answer.
Francesco Pugliese
Hello Francesco,
I will close this thread because of your similar question in a following thread.
Bes Regards,
Helfried