Part Number: WL1835MODCOM8B
Other Parts Discussed in Thread: TMDXEVM3358,
I am following the guide found here https://www.ti.com/lit/ug/swru581/swru581.pdf?ts=1618874311696&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FCC2564MODN
I'm using the AM335x EVM with the WL1835MODCOM8 card.
I am using the bt 4.2 linux add on found here https://www.ti.com/tool/TI-BT-4-2-STACK-LINUX-ADDON
I am using the bts file found here: https://www.ti.com/tool/WL18XX-BT-SP.
I have
root@am335x-evm:~/BluetopiaPM# ./LinuxSPPM
SPPM>1 1
BTPM_Initialize() Success: 0.
DEVM_RegisterEventCallback() Success: 5.
SPPM>9 1
echo 0 > /sys/class/gpio/gpio117/value
echo 1 > /sys/class/gpio/gpio117/value
echo 0 > /sys/class/gpio/gpio117/value
echo 1 > /sys/class/gpio/gpio117/value
BT COMM PORT (/dev/ttyS1): 6
Changing HCI baud rate to 3000000
Status: Executing BTS Script /lib/firmware/TIInit_11.8.32.bts.
Status: BTS Script successfully executed.
DEVM_PowerOnDevice() Failure: -4, Unknown Error.
Function Error.
SPPM>
running systemctl status bluetooth
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: Starting SDP server
Apr 19 20:50:07 am335x-evm systemd[1]: Started Bluetooth service.
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: bluetoothd[1465]: Failed to open control socket: Protocol not supported (93)
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: bluetoothd[1465]: Can't init bnep module
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: bluetoothd[1465]: Failed to init network plugin
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: [[0;1;31mFailed to open control socket: Protocol not supported (93)[[0m
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: bluetoothd[1465]: Bluetooth Management interface initialized
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: [[0;1;31mCan't init bnep module[[0m
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: [[0;1;31mFailed to init network plugin[[0m
Apr 19 20:50:07 am335x-evm bluetoothd[1465]: Bluetooth Management interface initialized