Part Number: WL1837MODCOM8I
Hallo everyone,
I am currently working on a project which includes precise time synchronization over Wlan. I got from my supervisor the following paper:
https://www.ti.com/lit/an/swaa162a/swaa162a.pdf
I cannot achieve the time`s synchronization enabling. I`ve used the instructions from the point 3 of paper.
Has someone already replicated the paper? I am actually working with a beaglebone green wireless which mets the hardware requirement specified from the paper.
I know from the Integration part that I have to connect the specific GPIO( I think the GPIO 2_2) with the Sitara CPU & WiLink8 module? .I have soldered a line between those modules,
but I wonder if there is a form to know which pin of the WiLInk8 module has to be connected in order to set it up.
I would really appreciate any information regarding this topics.
Best regards,
Victor Robles.