Part Number: DLP-7970ABP
Other Parts Discussed in Thread: MSP-EXP430F5529LP, , TRF7970A
I'm running some testing using the DLP-7970ABP and the MSP-EXP430F5529LP and the example software for the DLP-7970ABP (SLOC297 Rev C). I'm evaluating the TRF7970A read range, so I'm wondering what its output power is set to in the sample code. In the code, I don't see where the chip status control register is set for 3.3V operation, so I'm not sure whether the 14.5dBm or 17dBm mode as specified by the TRF7970A datasheet is being used.